Indoor Navigation using Consumer Portable Devices in Cart/Stroller
- Sep 25, 2017
- 2 min read

CASE STUDY
In the past few years, the huge and rapid development of portable devices (e.g. smartphones) as well as the increase in the number of users motivated researchers to effectively use the various components of such devices to develop different applications.
One emerging application using smartphones is to navigate users in shopping centers or retail stores while they use a shopping cart or stroller. The smartphone could be placed in the cart/stroller, whether directly, or inside a bag or purse in the cart/stroller or attached/hanged to the cart/stroller while it is pushed or pulled.
Cart Navigation using portable devices is a challenging task since INS will not provide acceptable accuracy, and the conventional PDR is not appropriate to be applied to such case as the device is not on the user body or directly related to it. The required information can’t be obtained or extracted from the collected data without a pre-processing step using appropriate signal processing techniques and disturbance/noise filtering.
In this paper, an enhanced dead reckoning positioning technique for cart navigation using portable devices is proposed. The proposed technique for cart navigation relies on dead reckoning and uses data from accelerometers and gyroscopes sensors. Also, any available absolute positioning information, upon availability, can be integrated with the proposed cart dead reckoning technique for further enhancement to the navigation solution.
Various tests scenarios were conducted to assess the performance of the proposed cart dead reckoning technique. The datasets were collected by a variety of subjects using different types of carts and strollers with various smartphones in different orientations and misalignment angles at different speeds of users.
The obtained results for over 1000 cart/stroller data demonstrate the capabilities of the proposed technique and its suitability for retail stores indoor navigation using portable devices in cart/stroller. The proposed algorithm shows competitive positioning performance of the portable devices in cart in terms of accuracy, reliability, and availability.
Read the full paper here.




Interesting use case — dead reckoning with the phone bouncing around in a stroller or cart has got to be a nightmare for sensor fusion. The noise filtering alone probably eats up half the processing time. This reminds me of how sometimes the raw data is just too messy to work with directly, similar to how I've used the low quality image maker to intentionally degrade photos for a meme — it's all about understanding what the signal looks like after you've added distortion. I'd be curious to see how they handle the transition when the user picks the phone up mid-navigation, since the motion model would shift completely.
One of the best things about Run 3 is the creative gameplay that lets players run on walls and avoid dangerous gaps in space. The increasing difficulty keeps every level challenging and rewarding. It’s a fantastic browser game for casual and competitive gamers alike!
The concept is solid, but carts and strollers are brutal test cases. Phone orientation, bags, vibration, and random walking speeds can wreck weak positioning fast. I prefer tech that removes friction, like Mii Generator, which lets you make Mii-style avatars online without a console or registration.
Dead reckoning in a cart sounds neat, but the real pain is still messy sensor noise and weird phone placement. That’s where practical tools matter. I’d rather pair this kind of indoor-navigation data with something like Whisper Web — an in-browser speech-to-text tool that runs transcription locally, no uploads, useful for turning field-test notes, interviews, or demo recordings into text fast.
I keep coming back to Pixel Flow because every level feels readable, even when it’s hard. You’ve got the layered block object right in front of you, the conveyor queue coming in, the colors of the pigs, and the waiting slots counting down your room for error. There’s enough going on to make it tense, but it never feels like the game is hiding information. That matters to me.