top of page

The Evolution of Wearable Intelligence: Solving the Power Paradox with STRIDE 

Apr 29
3 min read

Updated: Jul 28


1. The Wearables Paradox: Beyond the "Accuracy First" Myth 


As the pace of our lives continues to accelerate, our reliance on wearable technology has shifted from a luxury to mainstream. Whether it is for emergency response personnel, monitoring a lone worker’s safety in a remote facility, tracking an elderly family member, a child, or a marathoner’s route under dense tree canopy, we expect these devices to be unfailingly accurate. 


However, there is a fundamental conflict at the heart of wearable design: The Paradox of Compatibility. Users want more features (health biometrics, real-time mapping, Augmented Reality (AR) overlays) and sleeker, more lightweight designs—but these features demand power. While engineers often obsess over positional accuracy, it is a secondary constraint.  In the wearable ecosystem, power is the ultimate arbiter of performance. 


2. Why Always-On GNSS is a Legacy Solution 


Most real-time positioning relies on the Global Navigation Satellite System (GNSS). To maintain a high-confidence "fix," a device must stay in constant communication with at least 4 to 6 satellites. 

For a wearable, this "always-on" state is unsustainable for three reasons: 

  1. Power Drain: Continuous GNSS connection is a heavy drain on battery, which is unsuitable for wearable devices given the tight power constraints.  

  2. Volumetric Constraints: To support continuous GNSS, manufacturers must include larger batteries, leading to the "bulky" designs that consumers increasingly reject and additional costs. 

  3. Signal Vulnerability: GNSS is easily "denied" by urban canyons, indoor environments, or heavy weather, meaning the device often burns maximum power searching for a signal that isn't there. 

Modern wearables require a new approach to positioning that maintains accuracy and availability when GNSS struggles and does not drain the device’s power supply so quickly.  


3. STRIDE & Duty-Cycling: A New Architecture for Longevity 


Rather than forcing a hardware-heavy solution, TDK Trusted Positioning launched STRIDE in January 2026. STRIDE moves away from constant GNSS reliance toward a hybrid model known as GNSS Duty-Cycling, through Pedestrian Dead Reckoning (PDR). 


How It Works: GNSS/INS Duty-Cycling 


STRIDE uses Inertial Navigation System (INS)—comprising the accelerometer, gyroscope, and magnetometer—to deliver 3D positioning, uncertainties, heading, speed & distance, and mode detection. Unlike GNSS, these sensors are "always-on" and consume significantly less power. 

  1. The INS Interval: During "GNSS-Off" periods, STRIDE’s PDR algorithms continue to deliver 3D positioning, uncertainties, heading, speed & distance, mode detection based. 

  2. The Correction Pulse: Periodically, STRIDE enables the GNSS to provide an absolute reference point, correcting any "drifts" that naturally occur with Pedestrian Dead Reckoning (PDR) 



4. Quantifying the Impact: The Efficiency Leap 


To understand the real-world impact, we can model a 20-second window comparing continuous tracking to a 10-second duty cycle. GNSS receivers typically require an "acquisition spike" to lock onto satellites before dropping to a steady tracking state.

 

  1. Continuous GNSS: 

  2. First 5s (Acquisition): 5s × 120 mW = 600 mWs 

  3. Next 15s (Tracking): 15s × 100 mW = 1500 mWs 

  4. Total Energy: 2.1Ws 

  5. STRIDE Duty-Cycling (10s ON / 10s OFF): 

  6. First 5s (Acquisition): 5s × 120 mW = 600mWs 

  7. Next 5s (Tracking): 5s × 100mW = 500mWs 

  8. Final 10s (GNSS OFF / INS Only): 10s × 0 mW 

  9. Total Energy: 1.1Ws


By intelligently cycling the GNSS, STRIDE achieves ~46% gross power savings. Even after factoring in the minimal processing required for PDR, the net efficiency gain remains the single most effective way to extend wearable battery life without hardware changes. 


5. Transforming the Industry: From Watches to Smart Glasses 


This shift from "hardware-dependent" to "software-intelligent" positioning is redefining what is possible in 2026: 

  1. Smart Glasses: STRIDE enables head-mounted devices such as glasses and helmets to overcome the compatibility paradox so they can now maintain spatial awareness in the most challenging GNSS-denied environments without compromising aesthetics or the user experience.  

  2. Lone Worker Safety: For personnel in remote, urban or mixed (outdoor/indoor) environments, STRIDE helps ensure they are never lost, providing a continuous connection even when satellites are blocked. 

  3. Elderly / Child Monitoring: STRIDE improves the safety and protection of our loved ones by extending battery life and improving accuracy for geofencing. 

  4. Sport & Fitness: High-fidelity route tracking is now possible on ultra-slim devices that can last for multi-day events on a single charge. 


6. The Future: Intelligence in Operation 


Finally, the Compatibility Paradox has been solved! The benchmark for a wearable is no longer how much energy it can store, but how intelligently it uses it. STRIDE represents a paradigm shift: moving high-power systems from 'always-on' to 'on-demand'. By evolving positioning into a persistent, low-power enabler, we are entering a new age of sleek, high-performance technology that truly serves the user, freeing humanity from previous limitations of the tools meant to empower us.  







bottom of page