Our Technology
Our Technology
Single Platform. Endless Applications.
Trusted Positioning Inc specializes in developing software-based positioning solutions that provide reliable, accurate, and continuous location tracking even in challenging environments where traditional GNSS (Global Navigation Satellite System) signals are degraded, blocked or unavailable (e.g. tunnels, urban canyons, indoor facilities).
Our core technology relies on sensor fusion, specifically integrating inertial sensor data (from MEMS accelerometers and gyroscopes) with GNSS, geomagnetic and other wireless signals (e.g. magnetometers, barometers, RADAR) to provide the best possible positioning in any environment.
Core Technology Pillars
Inertial Navigation systems (INS):
This is a critical part of our technology because inertial sensors (IMUs) are always active, providing relative positioning information that continues to function even when other signals (like GNSS) fail.
Sensor Fusion:
Our software intelligently gathers data from all available sources to filter out erroneous measurements and determine the most accurate position.
Embedded & Hardware-Agnostic:
Our solutions are designed as embedded software that runs on an existing application processor. They are hardware-independent, allowing them to be integrated into existing sensor suites without requiring additional hardware.
Platform Architecture
The Trusted Positioning platform is built using a modular, layered architecture that has evolved over decades of real-world deployment.
Sensor Ingestion Layer
Collects raw data from inertial sensors, GNSS, vehicle signals, and other available inputs.
Fusion & Estimation Layer
Applies motion models, calibration techniques, and probabilistic sensor fusion to maintain continuous positioning as signal quality and environments change.
Application Layer
Optimizes outputs for specific devices, motion profiles, and operational constraints - supporting everything from vehicles and wearables to robots and micromobility platforms.
This shared architecture is what enables one platform to scale across applications - without fragmentation or duplicated systems.

Platform Integration
All our products (TRACK, DRIVE, AUTO, RIDE, STRIDE, and VENUE) run as embedded software on the device, ensuring low latency and high reliability. It does not depend on cloud connectivity or dedicated hardware, giving OEMs maximum flexibility. If you would like more clarification about integrating this software into your platform, contact us.
Being an embedded software solution means there is no need to install specific hardware or a cloud service.
We are able to deliver position updates in real-time because our software does not need an app or Cloud service to operate. This ensures rapid and reliable results with minimal latency.
Our software is hardware-independent and software-agnostic, giving you the freedom and flexibility to choose the sensors or work with the existing ones.
The Trusted Positioning Platform
The core of all our technology lies in the Trusted Positioning Platform which ingests relative and absolute inputs to output a continuous, accurate position through our software.
Depending on the application, inputs may include:
Inertial sensors (IMUs)
GNSS
Vehicle signals
Vision and perception inputs
Contextual and motion models
The intelligence lives in the software - allowing systems to adapt dynamically while remaining hardware-flexible and power-efficient.
Sensor Fusion, Designed for Reality
Positioning in the real world is unpredictable. Signals drop. Environments shift. Devices move differently depending on how - and where - they’re used.
​
Trusted Positioning software continuously evaluates the quality of available inputs and dynamically weights them in real time. When one source becomes unreliable, others seamlessly compensate - maintaining continuity without interruption.
​
This approach enables:
Continuous operation when GNSS is obstructed or degraded
Adaptation to diverse motion profiles
Consistent results across form factors and environments
Strong performance using cost-effective hardware
Through software calibration and intelligent error management, the platform unlocks higher performance without requiring specialized or power-hungry sensors.
Single Platform. Endless Applications.
All Trusted Positioning solutions are built on the same underlying platform, sharing a common core while being configured for different applications.
Continuous Performance
Keep operations connected through GNSS dropouts and challenging environments.
Efficiency & Reliability
Track assets, vehicles, and equipment in real time, indoors and out.
Optimized Resources
Extend battery life, minimize hardware changes, and scale with ease.

As the core platform evolves, every solution benefits - ensuring long-term consistency and scalability.
Designed to Scale Across Devices and Ecosystems
Modern products rarely operate in isolation. A single workflow may span vehicles, wearables, phones, tools, and industrial equipment.
​
Trusted Positioning supports multi-device ecosystems, enabling a unified positioning layer across:

Vehicles and machinery

Wearables and consumer devices

Industrial tools and assets

Robots and autonomous systems
This platform-level approach allows organizations to expand into new applications without redesigning their positioning foundation.

Proven Technology
With 60M+ licenses delivered, adoption by enterprise and Fortune 500 organizations, and a portfolio backed by 100+ approved patents, the platform reflects decades of applied innovation - not experimentation.
​
The platform supports autonomous operation at scale - maintaining continuous positioning across fleets, devices, and systems without manual intervention. It is:
Whether launching something new or evolving an existing system, the platform is built to support production realities.
What This Means for Your Team
A single, proven platform delivers tangible advantages:
Shorter development cycles
Fewer parallel engineering efforts
Greater flexibility in hardware selection
Easier expansion into new markets and applications
A positioning foundation that evolves with your roadmap
A single platform also reduces integration risk and enables scalable growth after launch - making it easier to expand into new applications, regions, or devices over time.
​
Instead of rebuilding for every use case, teams can innovate faster - on top of a trusted core.

Endless Applications.
Positioning challenges vary by application - but the foundation doesn’t have to.
By building everything on a single, adaptable platform refined over decades and deployed at scale, Trusted Positioning enables innovation across industries without compromise.
​
Endless applications demand a foundation you don’t have to rethink every time.
​
One platform. Endless applications.