The Next ADAS Breakthrough Won’t Come From More Sensors Alone
Updated: Jul 24

As automakers and Tier 1s move from autonomy pilots to scalable vehicle platforms, the next competitive advantage may come from right-sized positioning software that supports control-grade performance without unnecessary hardware complexity.
The automotive industry is experiencing a profound convergence. Software-defined vehicles (SDVs), AI integration, connected mobility, and Advanced Driver Assistance Systems (ADAS) are all colliding at a single practical question.
For OEMs and Tier 1 suppliers, the challenge is no longer just, "What is technically possible in a controlled pilot?" It is, "What can be validated, integrated, commercialized, and scaled profitably today?"
The answers to these questions will define the next generation of mass-market mobility.
Glossary
ADAS: Advanced Driver Assistance Systems
AV: Autonomous Vehicle
GNSS: Global Navigation Satellite System
LiDAR: Light Detection And Ranging
OEM: Original Equipment Manufacturer
SDV: Software-Defined Vehicle
Tier 1: Direct supplier of automotive components/assemblies to the OEM
ADAS is the Near-Term Commercialization Layer
While the industry-wide hype initially surrounded fully autonomous, driverless vehicles, market realities have shifted the priority from premium, low-volume demos to scalable platforms. According to industry outlooks, the primary commercial opportunity for the foreseeable future lies firmly within ADAS and Level 2/Level 2+ systems.
This segment represents the industry's "happy medium." By keeping the human driver in control while leveraging technology to drastically reduce human error, Level 2+ systems offer an immediate, viable path to mass deployment.
The Cost of Autonomy is Forcing Architecture Discipline
Achieving this scale requires a radical departure from early autonomy development strategies. The initial reflex of the autonomous vehicle (AV) race was to solve problems by throwing more hardware at the vehicle—stacking expensive LiDARs, high-definition cameras, and ultra-high-end computing.
However, overbuilt sensor stacks limit commercial deployment. You cannot scale a mass-market vehicle platform if the sensor suite costs more than the rest of the car combined!
The industry is now entering an era of strict architecture discipline. OEMs are pursuing a “right-sized autonomy architecture”—one that maximizes the efficiency of every component and leverages intelligent software to do the heavy lifting, rather than adding redundant, cost-prohibitive hardware.
Positioning is Becoming a Control-Layer Problem
In a right-sized architecture, we must re-evaluate how we view positioning. A multitude of ADAS features exist already—from blind-spot monitoring and lane-keep assist, to adaptive cruise control. But at the heart of these features is a fundamental requirement: accurate, real-time location awareness and integrity monitoring.
Advanced safety systems do not just need to know what street the vehicle is on for a turn-by-turn display. They require absolute precision regarding:

Velocity: Knowing the precise speed of the vehicle instantly.

Orientation: Understanding pitch, roll, and heading to predict vehicle dynamics.

Vehicle-Relative Motion: Tracking exact movement within a lane or relative to hazards.
When positioning inputs feed directly into steering, braking, and acceleration loops, the data must be flawless, high-rate, and continuous.
The Real Test is Degraded Conditions
It is easy for a vehicle to maintain positioning under open skies with a clear GNSS fix. But real-world reliability matters far more than open-sky performance claims.
The true test of an ADAS platform happens in degraded GNSS environments:
Urban Canyons: Where tall buildings block or reflect GNSS signals (multipath interference).
Tunnels and Underpasses: Where satellite connectivity drops entirely.
Bridges and Overpasses: Where multi-level roads confuse standard GPS.
Industrial Sites & Off-Road Environments: Where traditional mapping infrastructure is non-existent.
When a vehicle enters a tunnel, lane-keeping and adaptive cruise control cannot simply disengage and hand control back to a startled driver. The control layer requires continuous, uninterrupted positioning data to maintain safety margins when GNSS is completely unavailable.
Safety and Validation are Raising the Bar
The push for better positioning is not just driven by consumer expectations; it is mandated by evolving safety standards. The regulatory environment is tightening, with updated testing protocols like Euro NCAP 2026 raising the bar for ADAS performance.
Regulatory bodies are shifting away from idealized track testing and moving toward evaluating how ADAS handles varied, chaotic, real-world conditions. To achieve top safety ratings, vehicles must demonstrate robust performance in poor weather, sudden signal dropouts, and complex urban scenarios. Passing these validation hurdles requires a positioning foundation that remains resilient when primary external sensors are compromised.
Why Software-Defined Vehicles Need Sensor-Agnostic Positioning
As the industry transitions to SDVs, decoupling hardware from software has become a core engineering requirement. OEMs and Tier 1s can no longer afford to lock themselves into proprietary, tightly coupled hardware-and-sensor ecosystems.
Instead, they need flexible, software-based positioning layers that can:
Adapt across diverse vehicle platforms (from economy models to premium lines).
Integrate seamlessly with different sensor suites and chipsets.
Be updated over-the-air (OTA) as algorithms improve.
A sensor-agnostic, software-driven approach to sensor fusion ensures that the vehicle’s positioning capabilities grow smarter over time without requiring physical hardware changes.
DRIVE Enables Scalable, Control-Grade Navigation
To solve this architectural challenge, the automotive industry requires a new class of technology—one that bridges the gap between basic telematics and expensive, full-scale inertial navigation systems. A prime example of this approach is DRIVE by Trusted Positioning.
DRIVE is an integrated GNSS + Inertial Navigation System (INS) software solution designed specifically for this critical middle ground. It addresses a glaring market gap:

"Between low-cost telematics and full autonomy-grade positioning systems, there is a growing need for control-grade positioning that is accurate, available, affordable, and scalable. DRIVE was built for that middle ground."
By utilizing advanced sensor fusion algorithms, DRIVE delivers control-grade accurate location awareness in real-time, even when GNSS is entirely unavailable. It provides the essential position, velocity, and orientation inputs required by advanced control systems, without the cost burden of full-scale inertial hardware or perception-heavy architectures.
Conclusion
The next breakthrough in ADAS will not be defined by adding a tenth camera or a third LiDAR to the vehicle. It will be defined by software intelligence—specifically, how effectively a vehicle can fuse its existing data to maintain absolute control-grade awareness in the toughest environments.
As we look toward a future of commercialization and monetization of SDVs, Trusted Positioning will be there to showcase how right-sized, sensor-agnostic software can power the next generation of ADAS, robotic, and semi-autonomous platforms.
We hope to discuss with you the ways we can help you build scalable, safe, and highly profitable vehicle platforms for the real world.